MMPF0100 POWERON

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MMPF0100 POWERON

跳至解决方案
2,067 次查看
atillametetured
Contributor V

Greetings,

On the Sabre board for Smart Devices of iMX6, the PMIC power on pin is connected to VSNVS rail and this confuses me. If PWRON pin is configured as level sensitive such that active high turns the device on, how can it turn itself on when is is not yet turned on and there is no voltage on the VSNVS output? Can someone explain? Perhaps I am misinterpreting the situation.

Regards,

Mete

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,746 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The PMIC VSNVS pin is connected to Li-cel, assuming it is always ON power,

or it is powered first during PMIC Start-up Sequence. Please refer to PMIC

Datasheet about its power up sequence.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,747 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The PMIC VSNVS pin is connected to Li-cel, assuming it is always ON power,

or it is powered first during PMIC Start-up Sequence. Please refer to PMIC

Datasheet about its power up sequence.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------