MMPF0100 POWERON

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 POWERON

Jump to solution
2,072 Views
atillametetured
Contributor V

Greetings,

On the Sabre board for Smart Devices of iMX6, the PMIC power on pin is connected to VSNVS rail and this confuses me. If PWRON pin is configured as level sensitive such that active high turns the device on, how can it turn itself on when is is not yet turned on and there is no voltage on the VSNVS output? Can someone explain? Perhaps I am misinterpreting the situation.

Regards,

Mete

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,751 Views
Yuri
NXP Employee
NXP Employee

Hello,

The PMIC VSNVS pin is connected to Li-cel, assuming it is always ON power,

or it is powered first during PMIC Start-up Sequence. Please refer to PMIC

Datasheet about its power up sequence.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,752 Views
Yuri
NXP Employee
NXP Employee

Hello,

The PMIC VSNVS pin is connected to Li-cel, assuming it is always ON power,

or it is powered first during PMIC Start-up Sequence. Please refer to PMIC

Datasheet about its power up sequence.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------