LWIP example is not working in BOARD_SDRAM(external RAM).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LWIP example is not working in BOARD_SDRAM(external RAM).

Jump to solution
1,806 Views
JainamShah
Contributor I

Hello,

I am working on the lwip_dhcp_freeRtos example. I have changed the default memory settings in example code to run the lwip stack in the external RAM. After doing this device can not be able to go into the bound state. I am attaching the configurations below.

Actually, I am using the LCD in my project which overflows the SDRAM_DTC segment. So, I have changed the memory settings as below. 

 

JainamShah_0-1690806992769.png

 

JainamShah_1-1690807005655.png

 

After changing this the DHCP state got stuck at the SELECTING state.  

JainamShah_2-1690807255806.png

 

Please help me to solve this issue. 

Thank you.

 

 

0 Kudos
Reply
1 Solution
1,786 Views
jingpan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
1 Reply
1,787 Views
jingpan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply