LWIP example is not working in BOARD_SDRAM(external RAM).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LWIP example is not working in BOARD_SDRAM(external RAM).

ソリューションへジャンプ
1,807件の閲覧回数
JainamShah
Contributor I

Hello,

I am working on the lwip_dhcp_freeRtos example. I have changed the default memory settings in example code to run the lwip stack in the external RAM. After doing this device can not be able to go into the bound state. I am attaching the configurations below.

Actually, I am using the LCD in my project which overflows the SDRAM_DTC segment. So, I have changed the memory settings as below. 

 

JainamShah_0-1690806992769.png

 

JainamShah_1-1690807005655.png

 

After changing this the DHCP state got stuck at the SELECTING state.  

JainamShah_2-1690807255806.png

 

Please help me to solve this issue. 

Thank you.

 

 

0 件の賞賛
返信
1 解決策
1,787件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
1 返信
1,788件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信