LCD display 4 small images when Starting kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LCD display 4 small images when Starting kernel

跳至解决方案
2,424 次查看
ganboshi
Contributor II

I am in trouble,

the RGB LCD display logo is normal in uboot and kernel, but the LCD flash 4 small images when from uboot to kernel about 300ms when starting kernel. the port of LVDS0_DATA0,LVDS0_DATA1,LVDS0_DATA2 have abnormal signal, but the port of LVDS0_CLK is normal through the Oscilloscope. 

 I use  I.MX6DL over LVDS port connect to TM035KBH02 transform RGB signal to 320x240 LCD.

My Linux environment is 4.1.15

I don't know what config is incorrect when start kernel, so i need some help, thanks a lot.

1.jpg

LVDS0_DATA0 waveform:

2.jpg

标签 (1)
0 项奖励
回复
1 解答
2,283 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ganbo

please try patches from

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

and nxp linux

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,284 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ganbo

please try patches from

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

and nxp linux

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,283 次查看
ganboshi
Contributor II

Hi igor

Thanks for your support, I have fix my problem after use the 4.1.15 patch.

0 项奖励
回复