LCD display 4 small images when Starting kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD display 4 small images when Starting kernel

ソリューションへジャンプ
3,353件の閲覧回数
ganboshi
Contributor II

I am in trouble,

the RGB LCD display logo is normal in uboot and kernel, but the LCD flash 4 small images when from uboot to kernel about 300ms when starting kernel. the port of LVDS0_DATA0,LVDS0_DATA1,LVDS0_DATA2 have abnormal signal, but the port of LVDS0_CLK is normal through the Oscilloscope. 

 I use  I.MX6DL over LVDS port connect to TM035KBH02 transform RGB signal to 320x240 LCD.

My Linux environment is 4.1.15

I don't know what config is incorrect when start kernel, so i need some help, thanks a lot.

1.jpg

LVDS0_DATA0 waveform:

2.jpg

ラベル(1)
0 件の賞賛
返信
1 解決策
3,212件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganbo

please try patches from

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

and nxp linux

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,213件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganbo

please try patches from

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

and nxp linux

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,212件の閲覧回数
ganboshi
Contributor II

Hi igor

Thanks for your support, I have fix my problem after use the 4.1.15 patch.

0 件の賞賛
返信