Kernel getting tainted in Zeus when integrating bcmdhd driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel getting tainted in Zeus when integrating bcmdhd driver

1,344 Views
sd05
Contributor III

I am trying to integrate the bcmdhd driver in the Zeus linux-imx kernel, getting linking error for wifi_card_detect and sdio_reset_conn symbols, so I tried to add definition as per the earlier version this solves the compilation issue. But when I am getting issue in card detection when I tried to load module, the kernel is getting tainted(refer the logs )
I am using - imx6ull based custom board 

0 Kudos
Reply
1 Reply

1,339 Views
igorpadykov
NXP Employee
NXP Employee

Hi sd05

 

for tainted kernel issue may be useful to look at

https://support.hpe.com/hpesc/public/docDisplay?docId=c02905321&docLocale=en_US

 

Best regards
igor

0 Kudos
Reply