Kernel getting tainted in Zeus when integrating bcmdhd driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel getting tainted in Zeus when integrating bcmdhd driver

1,388 次查看
sd05
Contributor III

I am trying to integrate the bcmdhd driver in the Zeus linux-imx kernel, getting linking error for wifi_card_detect and sdio_reset_conn symbols, so I tried to add definition as per the earlier version this solves the compilation issue. But when I am getting issue in card detection when I tried to load module, the kernel is getting tainted(refer the logs )
I am using - imx6ull based custom board 

0 项奖励
回复
1 回复

1,383 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sd05

 

for tainted kernel issue may be useful to look at

https://support.hpe.com/hpesc/public/docDisplay?docId=c02905321&docLocale=en_US

 

Best regards
igor

0 项奖励
回复