Is there any problem if i.MX6 Dual VDD_ARM23_xx connection are same as i.MX6 Quad?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any problem if i.MX6 Dual VDD_ARM23_xx connection are same as i.MX6 Quad?

跳至解决方案
3,280 次查看
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm about i.MX6 Dual power supply.

Actually, on our custom board, connection of VDD_ARM23_IN pins and VDD_ARM23_CAP pins  are following.

(our connection is not changed from i.MX6Q connection even though we use i.MX6 "Dual")

In this case, is there any problem?

(e.g. chip will be dameged, power consumption will be increased, no problem, etc...)

[Connection]

VDD_ARM23_IN: 1.375V from MMPF0100 is supplied same as i.MX6Q connection.

VDD_ARM23_CAP: connect to VDD_ARM_CAP same as i.MX6Q connection.

Best Regards,

Satoshi Shimoda

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,855 次查看
VladanJovanovic
NXP Employee
NXP Employee

Yes, that is correct.

You can find gudelines for designing common circuit to accept all 4 i.MX 6 variants here:

http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf

br,

Vladan

在原帖中查看解决方案

0 项奖励
回复
9 回复数
2,855 次查看
fabio_estevam
NXP Employee
NXP Employee

Please check the mx6q datasheet, "4.1.3 Operating Ranges", note 2 states the following about VDD_ARM23_IN connection for quad and dual:

"For Quad core system, connect to VDD_ARM_IN. For Dual core system, may be shorted to GND together with

VDD_ARM23_CAP to reduce leakage."

Regards,

Fabio Estevam

2,855 次查看
satoshishimoda
Senior Contributor I

Hi Fabio Estevam,

Sorry, I modified this question immediately before you sent a reply.

Can I apply your answer to not only VDD_ARM23_IN but also VDD_ARM_CAP?

According to the datasheet, the leakage is increase if i.MX6 Dual connection is same as i.MX6Q, but i.MX6 Dual is NOT damaged.

Is this understanding correct?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
2,856 次查看
VladanJovanovic
NXP Employee
NXP Employee

Yes, that is correct.

You can find gudelines for designing common circuit to accept all 4 i.MX 6 variants here:

http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf

br,

Vladan

0 项奖励
回复
2,855 次查看
yuhe-r64908
NXP Employee
NXP Employee

Hi Vladan,

The customer is waiting for the answer. Could you please help with it


Thanks,

Yu

0 项奖励
回复
2,855 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

guillermoron can you help with this case?

0 项奖励
回复
2,855 次查看
satoshishimoda
Senior Contributor I

Hi Vladan,

Thank you for your quick response.

OK, I understand the impact is only leakage.

Best Regards,

Satoshi Shimoda

0 项奖励
回复
2,855 次查看
satoshishimoda
Senior Contributor I

Do you have a data how much leakage is increased in the case?

I want to estimate it to adapt our product to EuP.

Best Regards,

Satoshi Shimoda

0 项奖励
回复
2,855 次查看
VladanJovanovic
NXP Employee
NXP Employee

Hi,

I don't know if we have done such measurements in detail to provide full details over temperature etc. But I have seen comments that, based on few measurements done, it is worth while following recommended design. Leakage range will be about 15-20mA at room temperature, and increasing at higher temperatures.

Best regards,

Vladan

2,855 次查看
satoshishimoda
Senior Contributor I

Hi Vladan,

Thank you for teaching the helpful data.
OK, I understand the leakage range.

Thank you for your cooperation.

Best Regards,

Satoshi Shimoda

0 项奖励
回复