Is there any problem if i.MX6 Dual VDD_ARM23_xx connection are same as i.MX6 Quad?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any problem if i.MX6 Dual VDD_ARM23_xx connection are same as i.MX6 Quad?

ソリューションへジャンプ
3,091件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm about i.MX6 Dual power supply.

Actually, on our custom board, connection of VDD_ARM23_IN pins and VDD_ARM23_CAP pins  are following.

(our connection is not changed from i.MX6Q connection even though we use i.MX6 "Dual")

In this case, is there any problem?

(e.g. chip will be dameged, power consumption will be increased, no problem, etc...)

[Connection]

VDD_ARM23_IN: 1.375V from MMPF0100 is supplied same as i.MX6Q connection.

VDD_ARM23_CAP: connect to VDD_ARM_CAP same as i.MX6Q connection.

Best Regards,

Satoshi Shimoda

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,666件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Yes, that is correct.

You can find gudelines for designing common circuit to accept all 4 i.MX 6 variants here:

http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf

br,

Vladan

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
2,666件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Please check the mx6q datasheet, "4.1.3 Operating Ranges", note 2 states the following about VDD_ARM23_IN connection for quad and dual:

"For Quad core system, connect to VDD_ARM_IN. For Dual core system, may be shorted to GND together with

VDD_ARM23_CAP to reduce leakage."

Regards,

Fabio Estevam

2,666件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Fabio Estevam,

Sorry, I modified this question immediately before you sent a reply.

Can I apply your answer to not only VDD_ARM23_IN but also VDD_ARM_CAP?

According to the datasheet, the leakage is increase if i.MX6 Dual connection is same as i.MX6Q, but i.MX6 Dual is NOT damaged.

Is this understanding correct?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
2,667件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Yes, that is correct.

You can find gudelines for designing common circuit to accept all 4 i.MX 6 variants here:

http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf

br,

Vladan

0 件の賞賛
返信
2,666件の閲覧回数
yuhe-r64908
NXP Employee
NXP Employee

Hi Vladan,

The customer is waiting for the answer. Could you please help with it


Thanks,

Yu

0 件の賞賛
返信
2,666件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

guillermoron can you help with this case?

0 件の賞賛
返信
2,666件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Vladan,

Thank you for your quick response.

OK, I understand the impact is only leakage.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
2,666件の閲覧回数
satoshishimoda
Senior Contributor I

Do you have a data how much leakage is increased in the case?

I want to estimate it to adapt our product to EuP.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
2,666件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Hi,

I don't know if we have done such measurements in detail to provide full details over temperature etc. But I have seen comments that, based on few measurements done, it is worth while following recommended design. Leakage range will be about 15-20mA at room temperature, and increasing at higher temperatures.

Best regards,

Vladan

2,666件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Vladan,

Thank you for teaching the helpful data.
OK, I understand the leakage range.

Thank you for your cooperation.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信