i.MX25 Boot:Mysterious phenomenon

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX25 Boot:Mysterious phenomenon

549 Views
HitoshiOgasawar
Contributor III

Dear Sir,

Our customers will have to question the behavior of the Boot "i.MX25".

Someone, the information!

I use DDR2.

Writing a 0xFFFF_FFFF to this 0x8000_0080 of DDR2, and asserted 'L' the POR_B.

Then, negates the 'H' in the POR_B within 1sec, I hope BOOT BOOT start but does not start.

The similar phenomenon Writing 0x0000_0000 the write value.

However, to start the BOOT is selected by writing "value 0xFFFF_FFFF, of 0x0000_0000 other than".

So I have a question.

Q1.

By writing the 0x0000_0000 or 0xFFFF_FFFF to 0x8000_0080 address is protected?

Q2.

When the Boot, Is there a 0x8000_0080 address that will affect?

Best Regards,

Jin.

0 Kudos
1 Reply

508 Views
HitoshiOgasawar
Contributor III

Dear Sir,

The cancellation since the matter resolved.

Best Regards,

JIn.

0 Kudos