Is iMX 6 SoloX with two WiFi module working simultaneously?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is iMX 6 SoloX with two WiFi module working simultaneously?

ソリューションへジャンプ
2,109件の閲覧回数
andy_kim
Contributor IV
Hello, I am going to apply two WiFi module to i.MX 6 SoloX SD2 and SD3. One WiFi module is connected to SD2 as Input and the other is connected to SD3 as Output. I wonder if SDK of i.MX 6 SoloX supports the operating of two WiFi module at the same time. Thanks, Andy
0 件の賞賛
返信
1 解決策
2,090件の閲覧回数
art
NXP Employee
NXP Employee

There seems to be no experience of connecting two WiFi modules to a single i.MX6
series processor. However, there should be no problem from the hardware point
of view if correctly configuring a driver instance bindings.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,091件の閲覧回数
art
NXP Employee
NXP Employee

There seems to be no experience of connecting two WiFi modules to a single i.MX6
series processor. However, there should be no problem from the hardware point
of view if correctly configuring a driver instance bindings.

0 件の賞賛
返信
2,083件の閲覧回数
andy_kim
Contributor IV

Hello,

 

Thanks for your confirmation.

 

BR,

Andy

0 件の賞賛
返信