Is iMX 6 SoloX with two WiFi module working simultaneously?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is iMX 6 SoloX with two WiFi module working simultaneously?

跳至解决方案
1,307 次查看
andy_kim
Contributor IV
Hello, I am going to apply two WiFi module to i.MX 6 SoloX SD2 and SD3. One WiFi module is connected to SD2 as Input and the other is connected to SD3 as Output. I wonder if SDK of i.MX 6 SoloX supports the operating of two WiFi module at the same time. Thanks, Andy
0 项奖励
回复
1 解答
1,288 次查看
art
NXP Employee
NXP Employee

There seems to be no experience of connecting two WiFi modules to a single i.MX6
series processor. However, there should be no problem from the hardware point
of view if correctly configuring a driver instance bindings.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,289 次查看
art
NXP Employee
NXP Employee

There seems to be no experience of connecting two WiFi modules to a single i.MX6
series processor. However, there should be no problem from the hardware point
of view if correctly configuring a driver instance bindings.

0 项奖励
回复
1,281 次查看
andy_kim
Contributor IV

Hello,

 

Thanks for your confirmation.

 

BR,

Andy

0 项奖励
回复