Is iMX 6 SoloX with two WiFi module working simultaneously?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is iMX 6 SoloX with two WiFi module working simultaneously?

Jump to solution
2,191 Views
andy_kim
Contributor IV
Hello, I am going to apply two WiFi module to i.MX 6 SoloX SD2 and SD3. One WiFi module is connected to SD2 as Input and the other is connected to SD3 as Output. I wonder if SDK of i.MX 6 SoloX supports the operating of two WiFi module at the same time. Thanks, Andy
0 Kudos
Reply
1 Solution
2,172 Views
art
NXP Employee
NXP Employee

There seems to be no experience of connecting two WiFi modules to a single i.MX6
series processor. However, there should be no problem from the hardware point
of view if correctly configuring a driver instance bindings.

View solution in original post

0 Kudos
Reply
2 Replies
2,173 Views
art
NXP Employee
NXP Employee

There seems to be no experience of connecting two WiFi modules to a single i.MX6
series processor. However, there should be no problem from the hardware point
of view if correctly configuring a driver instance bindings.

0 Kudos
Reply
2,165 Views
andy_kim
Contributor IV

Hello,

 

Thanks for your confirmation.

 

BR,

Andy

0 Kudos
Reply