IMX6Q LVDS split mode color wrong.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q LVDS split mode color wrong.

2,869 Views
比特卡
Contributor I

Hi,

In my imx6q board, I use 2 lvds channels to support 1920X720. The dts file is modified as below:

mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB24";
default_bpp = <32>;
。。。
};

&ldb {
status = "okay";
split-mode;

lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
primary;
status = "okay";

display-timings {
native-mode = <&timing0>;
timing0: hsd100pxn1 {
clock-frequency = <170000000>;
hactive = <1920>;
vactive = <720>;
hback-porch = <40>;
hfront-porch = <20>;
vback-porch = <40>;
vfront-porch = <20>;
hsync-len = <4>;
vsync-len = <12>;
};
};
};

lvds-channel@1 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";

display-timings {
native-mode = <&timing1>;
timing1: hsd100pxn1 {
clock-frequency = <170000000>;
hactive = <1920>;
vactive = <720>;
hback-porch = <40>;
hfront-porch = <20>;
vback-porch = <40>;
vfront-porch = <20>;
hsync-len = <4>;
vsync-len = <12>;
};
};
};
};

And the UBoot bootargs is:

setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=ldb,if=RGB32,bbp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off'

I use  Yocto,and BSP version is  L4.9.11。

The screen is Hannstart HSD123KPW2-D10。(datasheet is attached below.)

The wrong color(my board+lvds) and right color(MCIMX6Q-SDB+HDMI) snapshot pics are attached.

below is right color in MCIMX6Q-SDB+HDMI

hdmi-right-color.jpg

below is wrong color in my board. The two systems have the same kernel and rootfs.
lvds-wrong-color.jpg
I have tried some parameters in dts file, the problem still exist.
Could you please provide some advice?
Thanks a million! 
Labels (1)
0 Kudos
Reply
3 Replies

2,557 Views
比特卡
Contributor I

This issue has been fixed. The root cause is LVDS DATA line inverted. 

0 Kudos
Reply

2,557 Views
igorpadykov
NXP Employee
NXP Employee

Hi

for rgb24 usage with lvds one can look at below threads and adapt for own codes

iMX6QD How to Add 24-bit LVDS Support in Android 

https://community.nxp.com/thread/320314#comments 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,557 Views
比特卡
Contributor I

hi,Igorpadykov,

Thank You for your help!

The problem which I'm facing is like below:

https://community.nxp.com/thread/384484 

Thanks alot!

0 Kudos
Reply