IMX6Q LVDS split mode color wrong.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q LVDS split mode color wrong.

3,913件の閲覧回数
比特卡
Contributor I

Hi,

In my imx6q board, I use 2 lvds channels to support 1920X720. The dts file is modified as below:

mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB24";
default_bpp = <32>;
。。。
};

&ldb {
status = "okay";
split-mode;

lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
primary;
status = "okay";

display-timings {
native-mode = <&timing0>;
timing0: hsd100pxn1 {
clock-frequency = <170000000>;
hactive = <1920>;
vactive = <720>;
hback-porch = <40>;
hfront-porch = <20>;
vback-porch = <40>;
vfront-porch = <20>;
hsync-len = <4>;
vsync-len = <12>;
};
};
};

lvds-channel@1 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";

display-timings {
native-mode = <&timing1>;
timing1: hsd100pxn1 {
clock-frequency = <170000000>;
hactive = <1920>;
vactive = <720>;
hback-porch = <40>;
hfront-porch = <20>;
vback-porch = <40>;
vfront-porch = <20>;
hsync-len = <4>;
vsync-len = <12>;
};
};
};
};

And the UBoot bootargs is:

setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=ldb,if=RGB32,bbp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off'

I use  Yocto,and BSP version is  L4.9.11。

The screen is Hannstart HSD123KPW2-D10。(datasheet is attached below.)

The wrong color(my board+lvds) and right color(MCIMX6Q-SDB+HDMI) snapshot pics are attached.

below is right color in MCIMX6Q-SDB+HDMI

hdmi-right-color.jpg

below is wrong color in my board. The two systems have the same kernel and rootfs.
lvds-wrong-color.jpg
I have tried some parameters in dts file, the problem still exist.
Could you please provide some advice?
Thanks a million! 
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,601件の閲覧回数
比特卡
Contributor I

This issue has been fixed. The root cause is LVDS DATA line inverted. 

0 件の賞賛
返信

3,601件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

for rgb24 usage with lvds one can look at below threads and adapt for own codes

iMX6QD How to Add 24-bit LVDS Support in Android 

https://community.nxp.com/thread/320314#comments 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,601件の閲覧回数
比特卡
Contributor I

hi,Igorpadykov,

Thank You for your help!

The problem which I'm facing is like below:

https://community.nxp.com/thread/384484 

Thanks alot!

0 件の賞賛
返信