IMX6 CSI BT656 640x480 interlaced support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 CSI BT656 640x480 interlaced support

ソリューションへジャンプ
2,551件の閲覧回数
abeeshmp_dct
Contributor II

Hi Team,

Does imx6 CSI support 640x480 interlaced video in BT656 embedded SYNC protocol ?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,136件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes supported.

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,136件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ABEESH

unfortunately i.MX6SL does not support it, support was added in later

i.MX6 products with CSI module, please check for example DEINTERLACE_
STRIDE description in sect.19.7.12 CSI Frame Buffer Parameter Register
(CSI_CSIFBUF_PARA) i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,136件の閲覧回数
abeeshmp_dct
Contributor II

Hi igorpadykov,

Thank you very much for immediate reply.

In imx6, is that the limitation of CSI module or De-interlacing(VDIC) module.

BT656 640x480 Progressive mode is supported?

0 件の賞賛
返信
2,137件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes supported.

Best regards
igor

0 件の賞賛
返信
2,136件の閲覧回数
abeeshmp_dct
Contributor II

Thanks Igor.

0 件の賞賛
返信