Questions about iMX6Q ESAI TDM (network) mode external signal pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Questions about iMX6Q ESAI TDM (network) mode external signal pins

跳至解决方案
3,178 次查看
stevenlin001
Contributor II

Hi, 

I am trying to enable ESAI interface as TDM (network) mode for a multi-channel codec. 

I am looking at the IMX6DQRM.pdf 'Table 25-1. ESAI External Signals' as the attached images. The clock signals (CLK, FS, HF_CLK for both Tx/Rx) are very straightforward, but I can't tell which two data signals(Tx/Rx) will be used by iMX6 ESAI TDM (network) mode. 

After configured ESAI to TDM mode, will Tx/Rx data signals been fixed to specific two data signals? 
If yes, which two data signasl should I use ? 
If not, how to select them or configure them? 

Thanks for the help, 
Steven Lin

1 解答
2,873 次查看
igorpadykov
NXP Employee
NXP Employee

Hi steven

usage of these pins are programmable, please look at sect.

25.2.2 Serial Transmit 1 Data Pin i.MX6DQ Reference Manual :


TX1 is used for transmitting data from the ESAI_TX1 serial transmit shift register.

from sect.25.2.3 Serial Transmit 2/Receive 3 Data Pin :

TX2_RX3 is used as the TX2 for transmitting data from the ESAI_TX2 serial transmit
shift register when programmed as a transmitter pin..

TX2_RX3 is an input when data is being received by the ESAI_RX3 shift register.

sect.25.6.14 Transmit Control Register (ESAI_TCR), ESAI_TCR bits TEn

enable the transfer of data from ESAI_TXn

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,874 次查看
igorpadykov
NXP Employee
NXP Employee

Hi steven

usage of these pins are programmable, please look at sect.

25.2.2 Serial Transmit 1 Data Pin i.MX6DQ Reference Manual :


TX1 is used for transmitting data from the ESAI_TX1 serial transmit shift register.

from sect.25.2.3 Serial Transmit 2/Receive 3 Data Pin :

TX2_RX3 is used as the TX2 for transmitting data from the ESAI_TX2 serial transmit
shift register when programmed as a transmitter pin..

TX2_RX3 is an input when data is being received by the ESAI_RX3 shift register.

sect.25.6.14 Transmit Control Register (ESAI_TCR), ESAI_TCR bits TEn

enable the transfer of data from ESAI_TXn

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,873 次查看
stevenlin001
Contributor II

Hi igor,

Thanks for the information about these pins are not fixed, they are

programmable. And I've figured out the answer of my last question 'how to

select them or configure them?', the "Transmit/Receive FIFO Configuration

Register (ESAI_TFCR / ESAI_RFCR)" can be used to select TDM Tx/Rx data

signal pins. FYI.

Thanks,

Steven

0 项奖励
回复