IMX6 CSI BT656 640x480 interlaced support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 CSI BT656 640x480 interlaced support

Jump to solution
1,678 Views
abeeshmp_dct
Contributor II

Hi Team,

Does imx6 CSI support 640x480 interlaced video in BT656 embedded SYNC protocol ?

Labels (1)
0 Kudos
Reply
1 Solution
1,263 Views
igorpadykov
NXP Employee
NXP Employee

yes supported.

Best regards
igor

View solution in original post

0 Kudos
Reply
4 Replies
1,263 Views
igorpadykov
NXP Employee
NXP Employee

Hi ABEESH

unfortunately i.MX6SL does not support it, support was added in later

i.MX6 products with CSI module, please check for example DEINTERLACE_
STRIDE description in sect.19.7.12 CSI Frame Buffer Parameter Register
(CSI_CSIFBUF_PARA) i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,263 Views
abeeshmp_dct
Contributor II

Hi igorpadykov,

Thank you very much for immediate reply.

In imx6, is that the limitation of CSI module or De-interlacing(VDIC) module.

BT656 640x480 Progressive mode is supported?

0 Kudos
Reply
1,264 Views
igorpadykov
NXP Employee
NXP Employee

yes supported.

Best regards
igor

0 Kudos
Reply
1,263 Views
abeeshmp_dct
Contributor II

Thanks Igor.

0 Kudos
Reply