IMX50 features differentiation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX50 features differentiation

跳至解决方案
2,114 次查看
lyfsci
Contributor III

Hi Experts,

The product comparison link http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=IMX50_FAMILY&cof=0&am=0&mvf=p31~USB&eop=i... contains the column "Serial Interface Type" each of the parts specifying ethernet/USB/SPi.

What is the definition of the column provided ?

标签 (1)
0 项奖励
回复
1 解答
2,063 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,064 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
2,063 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lyf

all parts are identical (link column provided is not accurate), differencies

are given in IMX50CEC p.8

IMX50CEC   rev.7   10_2013.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复