IMX50 features differentiation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX50 features differentiation

ソリューションへジャンプ
2,120件の閲覧回数
lyfsci
Contributor III

Hi Experts,

The product comparison link http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=IMX50_FAMILY&cof=0&am=0&mvf=p31~USB&eop=i... contains the column "Serial Interface Type" each of the parts specifying ethernet/USB/SPi.

What is the definition of the column provided ?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,069件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,070件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,069件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

all parts are identical (link column provided is not accurate), differencies

are given in IMX50CEC p.8

IMX50CEC   rev.7   10_2013.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信