IMX50 features differentiation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX50 features differentiation

Jump to solution
2,119 Views
lyfsci
Contributor III

Hi Experts,

The product comparison link http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=IMX50_FAMILY&cof=0&am=0&mvf=p31~USB&eop=i... contains the column "Serial Interface Type" each of the parts specifying ethernet/USB/SPi.

What is the definition of the column provided ?

Labels (1)
0 Kudos
Reply
1 Solution
2,068 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
2,069 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

all parts are identical (link column provided is not accurate), differencies

are given in IMX50CEC p.8

IMX50CEC   rev.7   10_2013.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply