I.MX53 QSB boot SD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,095件の閲覧回数
michaelcarrier
Contributor III

I have an I.MX53 Quick Start Board without an SD card to boot it. I downloaded MXIMX535-START-R-BSP-11-09_C executable which should burn an SD. But the program runs and at the Create Disk screen there are no disk selections to choose from. Any ideas? Or are their other procedures to burn an SD card?

0 件の賞賛
返信
1 解決策
2,722件の閲覧回数
4guin4g4
Contributor IV

You can burn it manually.

The file i.MX53_START_Linux_UserGuide.pdf describe the steps of how to do so, from a Linux host computer, on chapter

7. Using a Linux Host to Set Up an SD/MMC Card

You can find the document at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX536&nodeId=018rH3ZrDR988D&fpsp=1&...

inside of the compressed file:

IMX53_1103_LINUXDOCS_BUNDLE

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,723件の閲覧回数
4guin4g4
Contributor IV

You can burn it manually.

The file i.MX53_START_Linux_UserGuide.pdf describe the steps of how to do so, from a Linux host computer, on chapter

7. Using a Linux Host to Set Up an SD/MMC Card

You can find the document at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX536&nodeId=018rH3ZrDR988D&fpsp=1&...

inside of the compressed file:

IMX53_1103_LINUXDOCS_BUNDLE

0 件の賞賛
返信
2,722件の閲覧回数
guythepie
Contributor I

You need right click on it and 'Run as administrator'

Regards,

Guy

0 件の賞賛
返信