I.MX53 QSB boot SD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I.MX53 QSB boot SD

跳至解决方案
3,118 次查看
michaelcarrier
Contributor III

I have an I.MX53 Quick Start Board without an SD card to boot it. I downloaded MXIMX535-START-R-BSP-11-09_C executable which should burn an SD. But the program runs and at the Create Disk screen there are no disk selections to choose from. Any ideas? Or are their other procedures to burn an SD card?

0 项奖励
回复
1 解答
2,745 次查看
4guin4g4
Contributor IV

You can burn it manually.

The file i.MX53_START_Linux_UserGuide.pdf describe the steps of how to do so, from a Linux host computer, on chapter

7. Using a Linux Host to Set Up an SD/MMC Card

You can find the document at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX536&nodeId=018rH3ZrDR988D&fpsp=1&...

inside of the compressed file:

IMX53_1103_LINUXDOCS_BUNDLE

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,746 次查看
4guin4g4
Contributor IV

You can burn it manually.

The file i.MX53_START_Linux_UserGuide.pdf describe the steps of how to do so, from a Linux host computer, on chapter

7. Using a Linux Host to Set Up an SD/MMC Card

You can find the document at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX536&nodeId=018rH3ZrDR988D&fpsp=1&...

inside of the compressed file:

IMX53_1103_LINUXDOCS_BUNDLE

0 项奖励
回复
2,745 次查看
guythepie
Contributor I

You need right click on it and 'Run as administrator'

Regards,

Guy

0 项奖励
回复