DA9053 locked up and i.MX53 is not booting up.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DA9053 locked up and i.MX53 is not booting up.

Jump to solution
1,342 Views
maris_kalbergs
Contributor I

I am using patches-imx-2.6.35_11.09.01 kernel

During software system Reboot CPU hanged up. After reasserting power system was not able to boot up.

I have found patches: Linux kernel development

where is stated that there is possibility to lock down DA9053 with random write into registers. Now we have faced that PMIC is booting up with wrong output voltages VLDO8 (+3,27V instead of +1,8V), VLDO9 (+1,508V instead of +1,3V) and VBUCKPERI (+2,887V instead of +2,5V).

may be some you have experienced similar issue and knows how to read PMIC OTP preprogrammed values or how to make hardware reset.

We have tried to assert nSHUTDOWN pin and this doesn’t help.


Labels (2)
0 Kudos
Reply
1 Solution
803 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Maris,

What board are you using?

Have you tried nONKEY, GPI14 and GPI15 resets?

Unfortunately there's no easy way to read the OTP registers. You may need to contact Dialog directly to get the info you need to read these registers.

Best regards.

Jorge.

View solution in original post

0 Kudos
Reply
1 Reply
804 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Maris,

What board are you using?

Have you tried nONKEY, GPI14 and GPI15 resets?

Unfortunately there's no easy way to read the OTP registers. You may need to contact Dialog directly to get the info you need to read these registers.

Best regards.

Jorge.

0 Kudos
Reply