How to use the jtag on the i.mx28*

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the jtag on the i.mx28*

Jump to solution
2,802 Views
junma
Contributor I

Had one used the jtag on the i.mx28* to debug the hardwre of the i.mx28*?

I need help about this!

Thanks very much!

Labels (1)
0 Kudos
Reply
1 Solution
2,385 Views
Yuri
NXP Employee
NXP Employee

Hello

  To debug, using JTAG, it is needed to enter special boot mode (Wait JTAG
connection).  In this boot mode (6), the boot ROM enables the JTAG pins, waiting

(in infinite loop) for the debugger to release it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
2,386 Views
Yuri
NXP Employee
NXP Employee

Hello

  To debug, using JTAG, it is needed to enter special boot mode (Wait JTAG
connection).  In this boot mode (6), the boot ROM enables the JTAG pins, waiting

(in infinite loop) for the debugger to release it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,385 Views
junma
Contributor I

Thanks Yuri!

     The other question,indeed,i want to know is what kind of usb debug adapter recommended to debug the i.mx28* via jtag.

Thanks again!

jun

0 Kudos
Reply
2,385 Views
Yuri
NXP Employee
NXP Employee

Hello,

   

 Basically any JTAG tool, supporting ARM926 may be applied with i.MX28.

 

Please refer to the following regarding recommended tools :

 

i.MX286 Processors|Dual CAN|NXP 

 

 

The following may be helpful :

 

All Boards JTAG 

 

 

ARM has tested the i.MX28 EVK board and even has a specific drop down for it in

DS-5 tools.

 

The new JTAG and Trace unit is called DSTREAM. Information on it can be found at

DSTREAM – ARM Developer 

 

DS-5 is the new development environment for Linux and bare metal development.

 Information on it can be found at

 

DS-5 Development Studio – ARM Developer 

 

 

Also IAR may be considered.

 

IAR Embedded Workbench 

Regards,

Yuri.

2,385 Views
junma
Contributor I

Thanks very much ,Yuri!

0 Kudos
Reply