How to use the jtag on the i.mx28*

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use the jtag on the i.mx28*

ソリューションへジャンプ
2,845件の閲覧回数
junma
Contributor I

Had one used the jtag on the i.mx28* to debug the hardwre of the i.mx28*?

I need help about this!

Thanks very much!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,428件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  To debug, using JTAG, it is needed to enter special boot mode (Wait JTAG
connection).  In this boot mode (6), the boot ROM enables the JTAG pins, waiting

(in infinite loop) for the debugger to release it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,429件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  To debug, using JTAG, it is needed to enter special boot mode (Wait JTAG
connection).  In this boot mode (6), the boot ROM enables the JTAG pins, waiting

(in infinite loop) for the debugger to release it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,428件の閲覧回数
junma
Contributor I

Thanks Yuri!

     The other question,indeed,i want to know is what kind of usb debug adapter recommended to debug the i.mx28* via jtag.

Thanks again!

jun

0 件の賞賛
返信
2,428件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   

 Basically any JTAG tool, supporting ARM926 may be applied with i.MX28.

 

Please refer to the following regarding recommended tools :

 

i.MX286 Processors|Dual CAN|NXP 

 

 

The following may be helpful :

 

All Boards JTAG 

 

 

ARM has tested the i.MX28 EVK board and even has a specific drop down for it in

DS-5 tools.

 

The new JTAG and Trace unit is called DSTREAM. Information on it can be found at

DSTREAM – ARM Developer 

 

DS-5 is the new development environment for Linux and bare metal development.

 Information on it can be found at

 

DS-5 Development Studio – ARM Developer 

 

 

Also IAR may be considered.

 

IAR Embedded Workbench 

Regards,

Yuri.

2,428件の閲覧回数
junma
Contributor I

Thanks very much ,Yuri!

0 件の賞賛
返信