All Boards JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

All Boards JTAG

All Boards JTAG

Debugging with JTAG

JTAG was created to test populated circuit boards after manufacture. Nowadays, JTAG is primarilly used to access sub-blocks of integrated circuits and useful mechanism for debugging embedded systems.

When used as a debugging tool, an in-circuit emulator - which in turn uses JTAG as the transport mechanism - enables a programmer to access an on-chip debug module which is integrated into the CPU, via the JTAG interface. The debug module enables the programmer to debug the software of an embedded system.

Besides debugging, the second purpose of the JTAG interface is allowing device programmer hardware to transfer data into internal non-volatile device memory. Some device programmers serve a double purpose for programming as well as debugging the device. [Source: http://en.wikipedia.org]

All Boards Hardware Software

i.MX27 ADS Board Installing OpenOCD and GDB

All Boards Debugging Android

All Boards How To Understand JTAG BSDL

Tags (1)
Comments

Hi, the link in your document, All Boards Debugging Android

seems not accessible :

Unauthorized

   Access to this place or content is restricted.

You might want to take a look at this.

Regards

Sinan Akman

No ratings
Version history
Last update:
‎08-07-2012 01:02 PM
Updated by: