How to use the jtag on the i.mx28*

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use the jtag on the i.mx28*

跳至解决方案
2,848 次查看
junma
Contributor I

Had one used the jtag on the i.mx28* to debug the hardwre of the i.mx28*?

I need help about this!

Thanks very much!

标签 (1)
0 项奖励
回复
1 解答
2,431 次查看
Yuri
NXP Employee
NXP Employee

Hello

  To debug, using JTAG, it is needed to enter special boot mode (Wait JTAG
connection).  In this boot mode (6), the boot ROM enables the JTAG pins, waiting

(in infinite loop) for the debugger to release it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,432 次查看
Yuri
NXP Employee
NXP Employee

Hello

  To debug, using JTAG, it is needed to enter special boot mode (Wait JTAG
connection).  In this boot mode (6), the boot ROM enables the JTAG pins, waiting

(in infinite loop) for the debugger to release it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,431 次查看
junma
Contributor I

Thanks Yuri!

     The other question,indeed,i want to know is what kind of usb debug adapter recommended to debug the i.mx28* via jtag.

Thanks again!

jun

0 项奖励
回复
2,431 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   

 Basically any JTAG tool, supporting ARM926 may be applied with i.MX28.

 

Please refer to the following regarding recommended tools :

 

i.MX286 Processors|Dual CAN|NXP 

 

 

The following may be helpful :

 

All Boards JTAG 

 

 

ARM has tested the i.MX28 EVK board and even has a specific drop down for it in

DS-5 tools.

 

The new JTAG and Trace unit is called DSTREAM. Information on it can be found at

DSTREAM – ARM Developer 

 

DS-5 is the new development environment for Linux and bare metal development.

 Information on it can be found at

 

DS-5 Development Studio – ARM Developer 

 

 

Also IAR may be considered.

 

IAR Embedded Workbench 

Regards,

Yuri.

2,431 次查看
junma
Contributor I

Thanks very much ,Yuri!

0 项奖励
回复