How to use DDR-controller on i.MX 8QuadXPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use DDR-controller on i.MX 8QuadXPlus

1,024 Views
040869
Contributor I

Hello, team!

I want to use i.MX 8QuadXPlus CPU (MiMX8QX6AVLFZAC) with 2-rank chip memories LPDDR-4 1200 (1024Gx32bit).

DDR controller on this cpu will work fine normal work on this memory in formfactory with 2 chip select and 2 chanel (1024*(16+16)+1024*(16+16))?

0 Kudos
Reply
1 Reply

1,000 Views
igorpadykov
NXP Employee
NXP Employee

Hi Denis

yes such memory can be used. Also one can look at i.MX8QXP MEK example

i.MX 8QXP Design Files for the i.MX 8QXP MEK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply