Hi,
I am trying to find a 512MB Micron DDR3 chip for i.MX6SL. I can only find MT41K256M16TW -093 and -107 in current market. The NXP compatibility chart is suggesting MT41K256M16HA -125: E, which is difference speed grade.
And the i.MX6SL datasheet only mentioned DDR3-800. So I don't know if I can use -093 and -107 for it. Please suggest a part number for me..
Also, I am only using one DDR3 chip for the MCU. The ACC signals are pin to pin connection. Do I still need to terminate them to Vtt? Thanks.