How to use DDR-controller on i.MX 8QuadXPlus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use DDR-controller on i.MX 8QuadXPlus

1,095件の閲覧回数
040869
Contributor I

Hello, team!

I want to use i.MX 8QuadXPlus CPU (MiMX8QX6AVLFZAC) with 2-rank chip memories LPDDR-4 1200 (1024Gx32bit).

DDR controller on this cpu will work fine normal work on this memory in formfactory with 2 chip select and 2 chanel (1024*(16+16)+1024*(16+16))?

ラベル(1)
0 件の賞賛
返信
1 返信

1,071件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Denis

yes such memory can be used. Also one can look at i.MX8QXP MEK example

i.MX 8QXP Design Files for the i.MX 8QXP MEK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信