How to test the CSI interface over the target prototype board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test the CSI interface over the target prototype board

1,695 Views
adityanagal
Contributor III

Hi ,

I am writing the diagnostics for the IMX6 solo based Target prototype board  and I need to test the CSI interface over the target board. I  need to implement the test case is the user space application to test the CSI interface. Please

let me know how can I do that. Any reference piece of software will be very helpful. Thanks.

 

Regards,

Aditya

0 Kudos
Reply
1 Reply

1,529 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

one can use unit test package (folder /mxc_v4l2_test)

imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

for description please refer to sect.9.6 Unit Test attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply