How to test the EIM interface on the Target prototype board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to test the EIM interface on the Target prototype board

2,434件の閲覧回数
adityanagal
Contributor III

Hi ,

I am writing the diagnostics for the IMX6 solo based Target prototype board  and I need to test the EIM interface over the target board. I  need to implement the test case is the user space application to test the EIM interface. Please

let me know how can I do that. Any reference piece of software will be very helpful. Thanks.

Regards,

Aditya

0 件の賞賛
返信
1 返信

2,259件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

one can test with sdk on

https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

please refer to Chapter 7 Configuring the EIM Driver attached pdf file for description.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信