How to test the CSI interface over the target prototype board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to test the CSI interface over the target prototype board

2,316 次查看
adityanagal
Contributor III

Hi ,

I am writing the diagnostics for the IMX6 solo based Target prototype board  and I need to test the CSI interface over the target board. I  need to implement the test case is the user space application to test the CSI interface. Please

let me know how can I do that. Any reference piece of software will be very helpful. Thanks.

 

Regards,

Aditya

0 项奖励
回复
1 回复

2,150 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

one can use unit test package (folder /mxc_v4l2_test)

imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

for description please refer to sect.9.6 Unit Test attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复