Hi,
I am trying to reboot second A7 core from the first A7 core repeatedly. on the 8th attempt to boot the second A7 core system stops responding. I have attached a small piece of code that reproduces the issue with me. I have been building it using the codesourcery gnu tool chain using the following command.
$ arm-none-eabi-gcc -gdwarf-2 -mthumb-interwork -msoft-float -mcpu=cortex-a7 -T link_ram.ld main_freescale.c
Here is a brief description of the program attached.
Variable cpu1_boot_trig_cnt tells how many time Core 1 has been powered up.
Variable cpu1_boot_cnt tells how many time Core 1 has successfully been powered up.
board: MCIMX7 SABRE
Kernel or BSP: Bare metal
ToolChain: gcc version 6.2.0 (Sourcery CodeBench 2016.11-51)
Frequency of reproducible: Always
Steps to reproduce: Build the code load it on core 0 and let it run. When paused cpu1_boot_cnt is stuck at 7. on connecting second A7 core to JTAG. The cpu is in wage state, unable to access memory or registers trhough debug.
Regards,
Abbas Zaidi
Original Attachment has been moved to: bme.zip
Hi Zaidi
since stucking happens after several attempts one can assume that
this may be due to power reasons. One can try not to use GPC and
only stop/reset second core using SRC registers. If this helps, later one can
add delays after GPC power up/down to allow internal power supply to become
stable before proceeding next code execution. Another option to try to narrow
down issue, try to use internal ram (starting from 0x00910000).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
As you advised instead of using GPC now I am only using SRC registers (SRC_A7RCR1 and SRC_SCR) to enable/diasble core_1 and reset core_1, and the results are same. On the 8th reboot second core fails.
what do you mean by "core fails", if it hangs or jumps to
exception, if yes one can check stack pointer and debug it more.
Also one can try to run test from OCRAM, to check if this is cased by ddr memory.
Thanks JayTu,
I tried loading image with u-boot, i let it run for a while and when I connect the core 0 with JTAG. The results are same.
My u-boot version is U-Boot 2015.04-imx_v2015.04_4.1.15_1.0.0_ga+g384e1c1
Hi JayTu,
I have already attached the code in my original post with the command line to build it.
Its the same code. I load the generated binary to address 0x90100000 and then enter command
$ go 0x90100108
on u-boot.
Do i need to modify it for u-boot? Not sure what sort of modifications are needed.