The i.MX 8M reference manual mentions a JTAG_SMODE[1:0] and a SJC DISABLE e-fuse that are necessary to disable JTAG access. But I can't find the address or location of the fuses. Where can I find them? Is there some document describing it?
解決済! 解決策の投稿を見る。
 
					
				
		
 bernhardfink
		
			bernhardfink
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Here is the description of these fuse bits:
| Fuse Address | Fuse Name | Function | Setting | 
| 0x470[21] | SJC_DISABLE | Disable/Enable the Secure JTAG Controller module. This fuse is used to create highest JTAG security level, where JTAG is totally blocked. | 0 - Secure JTAG Controller is enabled 1 - Secure JTAG Controller is disabled | 
| 0x470[23:22] | JTAG_SMODE[1:0] | JTAG Security Mode. Controls the security mode of the JTAG debug interface | 00 - JTAG enable mode 01 - Secure JTAG mode 1x - No debug mode | 
Hi,
I have the exact same question, can someone let me know the answer please?
And I agree with what someone else has posted, it is not very useful when the answer results in a private email.
Regards,
Chris
 
					
				
		
 bernhardfink
		
			bernhardfink
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Here is the description of these fuse bits:
| Fuse Address | Fuse Name | Function | Setting | 
| 0x470[21] | SJC_DISABLE | Disable/Enable the Secure JTAG Controller module. This fuse is used to create highest JTAG security level, where JTAG is totally blocked. | 0 - Secure JTAG Controller is enabled 1 - Secure JTAG Controller is disabled | 
| 0x470[23:22] | JTAG_SMODE[1:0] | JTAG Security Mode. Controls the security mode of the JTAG debug interface | 00 - JTAG enable mode 01 - Secure JTAG mode 1x - No debug mode | 
Hi,
When we are read the bank 1 word 3 in I.MX8MPLUS after the U-BOOT ,we observe the below value.
Does it means ,Is JTAG is Disable?
You said that SJC_DISABLE and JTAG_SMODE are set high ,that means JTAG is Disable.
Does the I.MX8M fuse address are applicable for I.MX8MPLUS ?.
| Fuse Address | Fuse Name | Function | Setting | 
| 0x470[21] | SJC_DISABLE | Disable/Enable the Secure JTAG Controller module. This fuse is used to create highest JTAG security level, where JTAG is totally blocked. | 0 - Secure JTAG Controller is enabled 1 - Secure JTAG Controller is disabled | 
| 0x470[23:22] | JTAG_SMODE[1:0] | JTAG Security Mode. Controls the security mode of the JTAG debug interface | 00 - JTAG enable mode 01 - Secure JTAG mode 1x - No debug mode | 
 
					
				
		
 bernhardfink
		
			bernhardfink
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		You seem to have a closed part. All 3 relevant bits are set. Bit definitions and the location are valid for i.MX 8M Plus.
Make a crosscheck with a debugger, if you don't see any core appearing, then the JTAG is definitely closed.
Regards,
Bernhard.
1.How to enable JTAG Mode in I.MX8MPLUS ?
2.Is there any possibility to override that register in I.MX8MPLUS ? for I.MX6 a bit is mentioned to override JTAG_SMODE by setting the BOOT_CFG_LOCK bits as shown below?.
 
					
				
		
 bernhardfink
		
			bernhardfink
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Closed is closed. If there would a way to re-open it, the closed configuration wouldn't make sense. The OTP bits are really just one-time-programmable.
The alternative way to access the chip is the Serial Download Protocol (SDP) on the USB port.
According to your readout, bit[28] = BT_FUSE_SEL is not set, so the device can still boot taking a configuration from external BOOT_MODE pins.
Regards,
Bernhard.
Problem-1
1)We have I.MX8MP EVK has default image, stopped at u-boot using putty and checked below register JTAG
From above image JTAG Disable permanently one of of the NXP Support aslo given message.please confirm
Problem-2
1)We have custom board(i.MX8MP) doesnt have default image, any procedure for JTAG Access. Is it possible any where without default image JTAG access is possible????
2)If possible means how decribe procedure
3)if not, USB connections out cutstom device shown below
Its USB2.0 in EVK Type C connections given, said USB2.0 also compatible,then please given a procedure with our hardwrae and software loading using USB2.0.
Many days happen request you give clear and stright procedure for all of above
 
					
				
		
 bernhardfink
		
			bernhardfink
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		On my EVK boards the JTAG is enabled, the two lock bits are not set:
u-boot=>     fuse read 1 3
Reading bank 1:
Word 0x00000003: 88000000
1) The JTAG port on your EVK is disabled by the fuses.
2) The BOOT_MODE[3:0] pins need to have the value '0 0 0 1' to force the i.MX 8M Plus into serial downloader mode.
| Pin Name | Ball | Value for USB download | 
| BOOT_MODE0 | G10 | 1 | 
| BOOT_MODE1 | F8 | 0 | 
| BOOT_MODE2 | G8 | 0 | 
| BOOT_MODE3 | G12 | 0 | 
On the 8M Plus EVK this is easy to make, there are DIP switches near to the PWR switch, marked with BOOT_MODE.
The USB connection on your custom PCB seems to be perfectly fine, if you succeed to set the BOOT_MODE pins correctly, you should see the i.MX 8M Plus going into SDP mode after power-on:
Download the Windows UUU tool from here: https://github.com/nxp-imx/mfgtools/releases/download/uuu_1.5.201/uuu.exe
D:\Image-Programming>uuu.exe -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.201-0-g727fc2b
Connected Known USB Devices
        Path     Chip    Pro     Vid     Pid     BcdVersion      Serial_no
        ====================================================================
        2:6      MX865   SDPS:   0x1FC9 0x0146   0x0001  E5973000757D125C# Flash to SD-Card (if it's there)
> uuu.exe -b sd_all imx-image-full-imx8mpevk.wic
# Flash to eMMC
> uuu.exe -b emmc_all imx-image-full-imx8mpevk.wic# Download to RAM
> uuu.exe imx-boot-imx8mpevk-sd.bin-flash_evk
# Flash to SD-Card (if it's there)
> uuu.exe -b sd imx-boot-imx8mpevk-sd.bin-flash_evk
# Flash to eMMC
> uuu.exe -b emmc imx-boot-imx8mpevk-sd.bin-flash_evkRegards,
Bernhard.
Previous Post Image is not clear please check below
Hi @igorpadykov 
Could you forward to me details as well?
Kind regards,
Marcin
 
					
				
		
 bernhardfink
		
			bernhardfink
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Meanwhile these fuse bits have been documented in the Security Reference Manuals of 8M Nano and 8M Plus. It's the same structure as in 8M and 8M Mini.
I will check
Regards,
Bernhard.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Christian
one can look at
Understanding how to burn eFuses on i.MX8 and i.MX8x families - i.MXDev Blog
https://community.nxp.com/thread/505184
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
thanks for the reply. My problem is not how to set a fuse in general. It's more the problem where this specific fuses are located.
For example: The reference manual tells me that BT_FUSE_SEL is at 0x470[28] and it tells me that this is bank 1 word 3. But it doesn't tell me a location for JTAG_SMODE[1:0] and SJC DISABLE. For i.MX6 or i.MX7 there is another document that tells me the location (https://www.nxp.com/docs/en/application-note/AN4581.pdf ). But I didn't find one for i.MX8.
Best regards
Christian
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Christian
I sent additional details by mail.
Best regards
igor
Can you also send me the additional details?
Thank you.
 
					
				
		
 bernhardfink
		
			bernhardfink
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I marked my answer from last year as solution, so that it's easier to find.
Please post the solution here instead of sending it to one single recipient. There are too many threads here that end with "I sent you a mail". The thread is useless for everyone but the thread creator.
I would like to have this information as well.
Thanks,
Marcus
Hi Igor
Can you please send me the same information as well.
Thanks in advance,
TG
Thanks, igorpadykov, very helpful to answer this by mail!
How about others like us who are also wondering about all this?
Hello Igor,
thank you. That solved my question.
Best regards
Christian