How to / Can I get Qt version in yocto build updated?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to / Can I get Qt version in yocto build updated?

3,697 Views
abinjoseph
Contributor I

Hi all,

I have a Qt application developed in Qt 5.2.1, and now I need to run it on SabreSD board.

I have lost my pre-built image, and so I follow the steps in https://community.freescale.com/docs/DOC-94849 to build my application.

I found that Qt version in the BSP source is 4.8. Is there a way to update it?

Hope someone could help me to resolve this. Thanks :smileyhappy:

Tags (2)
0 Kudos
Reply
1 Reply

2,338 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abin

please look at

Qt 5.3.0 release on i.MX6 using fsl-community-bsp and meta-qt5

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply