How to / Can I get Qt version in yocto build updated?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to / Can I get Qt version in yocto build updated?

3,614 次查看
abinjoseph
Contributor I

Hi all,

I have a Qt application developed in Qt 5.2.1, and now I need to run it on SabreSD board.

I have lost my pre-built image, and so I follow the steps in https://community.freescale.com/docs/DOC-94849 to build my application.

I found that Qt version in the BSP source is 4.8. Is there a way to update it?

Hope someone could help me to resolve this. Thanks :smileyhappy:

标记 (2)
0 项奖励
回复
1 回复

2,255 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abin

please look at

Qt 5.3.0 release on i.MX6 using fsl-community-bsp and meta-qt5

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复