Ethernet and U-boot Environment variables

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet and U-boot Environment variables

1,759件の閲覧回数
saida
Contributor II

hi

i.mx community

this is my come back after small gap and i hope every community members are fine

for my i.mx6 sabresd board

1) how to modify ethernet driver in u-boot for my phy dp83848 TI chip

2) how i can port open source lwip TCP/IP stack to my custom board (i am not using OS, i want to make it standalone embedded system) so that my directly uses stack protocols.

3) sabre board doesn't have nor flash, environment variables are stored in MMC flash but in my board i have NOR flash where u-boot is stored and i want to store env in flash what are the modifications i have to do in u-boot.

this is my urgent requirement plz any one can give quick reply to me

thanks in advance

Regards

Saida

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,509件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Saida

1. seems dp83848 is already integrated on some i.MX6 boards, like fs-net PicoMODA9 board

2. lwip was in i.MX6 SDK, if you previously got it, then one can find it in sdk/lwip directory

  (also please find attached this part ).

3. this is defined in uboot/include/configs/  files, #define CONFIG_ENV_IS_IN_FLASH.

    For example one can look at mx6sabre_common.h

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信