How To Rotate 90 Degree Video For Display In I.MX8X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To Rotate 90 Degree Video For Display In I.MX8X

20,380 Views
alighieri
Contributor III

Here According To Datasheet And Reference Manual The New Follower Of I.MX Series Processor I.MX8X Is Designed Without IPU Which Is Built-In In Previous Series I.MX6 Processor. My Questions Is How To Rotate 90 / 180 Degree For Target Display In Wanted Orientation? Is Here Also Contain FRAMEBUFFER.C In BSP For Doing That?

0 Kudos
Reply
26 Replies

8,696 Views
alighieri
Contributor III

HI IGOR

Thank You For Your Kindly Help To Have Patch For I.MX8X Display Rotation. Looks The Feature Is Performed By GPU?

Bright

0 Kudos
Reply

8,009 Views
aber
Contributor III

hello alighieri

    Can you share the patch, thank you。

0 Kudos
Reply

6,249 Views
28658180
Contributor I

Hello,Bright

Will you please send me a copy of the patch? I met with the same problem, thanks

frank

0 Kudos
Reply

3,582 Views
aber
Contributor III

The system sets this property, and others can be changed as needed。

hwc.enable.overlay=0

 

0 Kudos
Reply

3,544 Views
jeniceks
Contributor I

Hello Aber

It seems your post is valid for android. How can I rotate screen (180 deg) on imx8x, linux without weston runnig QT application on eglfs plaform?

thx for help

0 Kudos
Reply

3,540 Views
aber
Contributor III

Hi jeniceks

    that configuration is for android, try configuring weston.ini under linux.

0 Kudos
Reply