Gaps between each 25 bytes in the spidev.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Gaps between each 25 bytes in the spidev.

879 次查看
r_gabdulhakov
Contributor I

Dear all,

I use a spidev device to write 200 bytes to spi.

Why are there gaps between every 25 bytes?

How to remove this gaps?

spidev.png

0 项奖励
回复
1 回复

824 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Renat

one can try to adjust BURST_LENGTH value of register ECSPIx_CONREG. If

this will not help, seems delays are caused by processor internal bus latencies

and unfortunately there is no way to change this.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复