Gaps between each 25 bytes in the spidev.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gaps between each 25 bytes in the spidev.

919件の閲覧回数
r_gabdulhakov
Contributor I

Dear all,

I use a spidev device to write 200 bytes to spi.

Why are there gaps between every 25 bytes?

How to remove this gaps?

spidev.png

0 件の賞賛
返信
1 返信

864件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Renat

one can try to adjust BURST_LENGTH value of register ECSPIx_CONREG. If

this will not help, seems delays are caused by processor internal bus latencies

and unfortunately there is no way to change this.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信