Layout suggestion for PF100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Layout suggestion for PF100

1,334件の閲覧回数
aabhishekoct18
Contributor III

Hi Team 

As  per  application notes  AN4717  pin no 48 of  PF100  is  GND  reference it should  be  keep away from high switching GND  reference  path   

pastedImage_1.png

But in layout  file  it is  connected  to GND  EP. Should  i caonnect this with GND  EP  or  connect to GND plane 

through separate via.

pastedImage_2.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,269件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abhishek

example of connection of pin no 48 of  PF100 can be found in  iMX6Q-SABRE-SDB-DESIGNFILES

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emu...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信