Gaps between each 25 bytes in the spidev.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gaps between each 25 bytes in the spidev.

588 Views
r_gabdulhakov
Contributor I

Dear all,

I use a spidev device to write 200 bytes to spi.

Why are there gaps between every 25 bytes?

How to remove this gaps?

spidev.png

0 Kudos
Reply
1 Reply

533 Views
igorpadykov
NXP Employee
NXP Employee

Hi Renat

one can try to adjust BURST_LENGTH value of register ECSPIx_CONREG. If

this will not help, seems delays are caused by processor internal bus latencies

and unfortunately there is no way to change this.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply