Frame Syncs are not in Phase

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Frame Syncs are not in Phase

跳至解决方案
1,588 次查看
sreedhar_appala
Contributor IV

Hi,

I am working with i.MX8MM EVK and another SoC is interfaced to the EVK hw.

The SAI1 of iMX8MM is Master and generating the Frame Sync.

This Frame Sync from SAI1 is connected to I2S In Port of SoC.

Internally in SoC this Frame Sync is routed to I2S Out port and it is used as Frame Sync of I2S Out

When we observe these two Frame Syncs (Frame Sync Generated by SAI1 and Frame Sync at I2S Out port) on CRO. they are not in phase.

Is there a way or any programming sequence of SAI registers can we achieve the similar phase? 

Because out of phase can lead us to sample swap issues.

Please let us know.

Thank you, Sreedhar

0 项奖励
回复
1 解答
1,577 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

 

I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay

(there is no such hardware settings in SAI module), sorry.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,578 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

 

I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay

(there is no such hardware settings in SAI module), sorry.

 

Best regards
igor

0 项奖励
回复
1,566 次查看
sreedhar_appala
Contributor IV

Thank you Igor !!

0 项奖励
回复