Frame Syncs are not in Phase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Frame Syncs are not in Phase

ソリューションへジャンプ
2,089件の閲覧回数
sreedhar_appala
Contributor III

Hi,

I am working with i.MX8MM EVK and another SoC is interfaced to the EVK hw.

The SAI1 of iMX8MM is Master and generating the Frame Sync.

This Frame Sync from SAI1 is connected to I2S In Port of SoC.

Internally in SoC this Frame Sync is routed to I2S Out port and it is used as Frame Sync of I2S Out

When we observe these two Frame Syncs (Frame Sync Generated by SAI1 and Frame Sync at I2S Out port) on CRO. they are not in phase.

Is there a way or any programming sequence of SAI registers can we achieve the similar phase? 

Because out of phase can lead us to sample swap issues.

Please let us know.

Thank you, Sreedhar

ラベル(3)
0 件の賞賛
返信
1 解決策
2,078件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

 

I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay

(there is no such hardware settings in SAI module), sorry.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,079件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

 

I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay

(there is no such hardware settings in SAI module), sorry.

 

Best regards
igor

0 件の賞賛
返信
2,067件の閲覧回数
sreedhar_appala
Contributor III

Thank you Igor !!

0 件の賞賛
返信