Frame Syncs are not in Phase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frame Syncs are not in Phase

Jump to solution
1,410 Views
sreedhar_appala
Contributor IV

Hi,

I am working with i.MX8MM EVK and another SoC is interfaced to the EVK hw.

The SAI1 of iMX8MM is Master and generating the Frame Sync.

This Frame Sync from SAI1 is connected to I2S In Port of SoC.

Internally in SoC this Frame Sync is routed to I2S Out port and it is used as Frame Sync of I2S Out

When we observe these two Frame Syncs (Frame Sync Generated by SAI1 and Frame Sync at I2S Out port) on CRO. they are not in phase.

Is there a way or any programming sequence of SAI registers can we achieve the similar phase? 

Because out of phase can lead us to sample swap issues.

Please let us know.

Thank you, Sreedhar

0 Kudos
Reply
1 Solution
1,399 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

 

I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay

(there is no such hardware settings in SAI module), sorry.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
1,400 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

 

I am afraid there is no way to adjust i.MX8MM SAI Frame Sync phase delay

(there is no such hardware settings in SAI module), sorry.

 

Best regards
igor

0 Kudos
Reply
1,388 Views
sreedhar_appala
Contributor IV

Thank you Igor !!

0 Kudos
Reply