Serial Downloader BOOT i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial Downloader BOOT i.MX6ULL

846 Views
ban45
Contributor III

Hi

(1) What should I do with BOOT via USB?

 

Should I connect it to a PC?
What kind of software (application) do you need?
Is there any equipment needed to connect, such as a debugger?

(2) What should I do with BOOT via UART?

Should I connect it to a PC?
What kind of software (application) do you need?
Is there any equipment needed to connect, such as a debugger?

Is there any difference from USB?

best regard

0 Kudos
Reply
1 Reply

840 Views
igorpadykov
NXP Employee
NXP Employee

Hi ban45

 

>(1) What should I do with BOOT via USB?

 

yes it is necessary to connect to usb, one can follow

Evaluation Kit based on i.MX 6ULL Quick Start Guide

and use uuu utility

https://github.com/NXPmicro/mfgtools

 

>(2) What should I do with BOOT via UART?

 

one can use Imx_usb_loader utility

https://variwiki.com/index.php?title=Imx_usb_loader

https://github.com/boundarydevices/imx_usb_loader

 

Best regards
igor

0 Kudos
Reply