FXOS8700 linux driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXOS8700 linux driver

2,759 Views
maximkuk
Contributor III

Hello!

In our custom board we use FXOS8700. When I start driver from fsl-arm-yocto-bsp (kernel 4.9.11), I see that it creates only one input device and event from accelerometer and magnetometer are emitting from one source, so I can't use acc and mag devices simultaneously.

I modifyed fxos8700 driver to create two input devices - separately for acc and mag. I think it will be useful to share this patch :smileyhappy:.

Labels (5)
0 Kudos
Reply
2 Replies

2,384 Views
pandaerliu
Contributor II

The patch fixed my problem.Thank you very much for sharing.

0 Kudos
Reply

2,384 Views
maximkuk
Contributor III

Or there is another version of this driver from here: https://community.nxp.com/thread/330614 

0 Kudos
Reply